Introduction to the Aquis Thin Client

This driver is a stand-alone driver. It provides additional functionality to enable ClearSCADA to interface with specific supported systems or devices. To interact successfully with such systems or devices, you need to:

Intended Audience

This guide is intended for engineers who are responsible for Aquis Serveritems and features in the ClearSCADA database.

Document Scope

This guide explains the configuration, features and database items that are specific to the Aquis Thin Client.

The AquisThin Client allows you to display real-life hydraulic optimization results when you are connected to a running web service of Aquis (Water Management). This web service allows you to browse and look up data and monitor attribute values (such as pressure, flow, and so on). The selection can be done for a stand-alone attribute or a time series. The Aquis Server offers read-only display of results from the server. The Aquis Server database item in ClearSCADA contains the URL link to the web service. Any configuration, including the server-side connection setup, is done on the Aquis application server.

The Aquis Thin Client is only available through ViewX and is not supported within WebX.


Disclaimer

ClearSCADA 2017 R3